Way of system reset by software

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Way of system reset by software

1,031件の閲覧回数
toshiharu_shimi
Contributor II

I would like to assert system reset by software.

I intend to use Software Reset Signal(SRS) in Watch dog Control Register, But errata report mentions that watchdog timeout or software trigger will not reset the SOC.

Is there other way to assert system reset by software?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

992件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Toshiharu

>Is there other way to assert system reset by software?

not, sorry. So recommendation is to remove power (Voltage source) to
all components on the board in the event of a processor reset.

NXP reference boards were designed to remove power (Voltage source)
to all components on the board in the event of a processor reset.

For example on i.MX7D Sabre SD schematic SPF-28590 p.23 

it is done with signal PMIC_PWRON, U37.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信