Way of system reset by software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Way of system reset by software

966 Views
toshiharu_shimi
Contributor II

I would like to assert system reset by software.

I intend to use Software Reset Signal(SRS) in Watch dog Control Register, But errata report mentions that watchdog timeout or software trigger will not reset the SOC.

Is there other way to assert system reset by software?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

927 Views
igorpadykov
NXP Employee
NXP Employee

Hi Toshiharu

>Is there other way to assert system reset by software?

not, sorry. So recommendation is to remove power (Voltage source) to
all components on the board in the event of a processor reset.

NXP reference boards were designed to remove power (Voltage source)
to all components on the board in the event of a processor reset.

For example on i.MX7D Sabre SD schematic SPF-28590 p.23 

it is done with signal PMIC_PWRON, U37.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply