Watchdog reset on imx6ul

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog reset on imx6ul

2,211 Views
pietercardoen
Contributor II

Dear

I am facing troubles with the watchdog on imx6ul. I am using u-boot 2016.03.

I configure:

* the WCR register to 0xFF34 (WDT and WDE enabled and timeout 128s)

* the WMCR register to 0x0000 (Power down counter disabled)

* the WSR to 0x5555 and afterwards to 0xaaaa

After 12 seconds, the board reboots and reset cause is WDOG.

If I change the timeout to 60 seconds, nothing changes. Also after 12 seconds, the board reboots.

What could cause this strange behaviour?

Best regards

Pieter

Labels (1)
0 Kudos
Reply
2 Replies

1,658 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pieter

reason may be that wdog was already initialized before, for example

in iROM by fuses, note that some wdog fields are write-once only.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,658 Views
pietercardoen
Contributor II

Igor

The issue was that the 32kHz clock was missing and apparently, the i.MX6UL behaved unpredictably. By adding this component, the WDOG behaves normal.

Best regards

Pieter Cardoen

0 Kudos
Reply