Watchdog as wakeup source in imx6ul

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog as wakeup source in imx6ul

1,804 Views
shammi112
Contributor I

Hello,

Is it possible to use watchdog as wake up source in imx6ul ?

Regards,

SHAMMI

Labels (1)
0 Kudos
Reply
5 Replies

1,572 Views
igorpadykov
NXP Employee
NXP Employee

Hi SHAMMI

yes any enabled interrupt can wake processor, for wdog one

can refer to sect.6.5.4.2 Interrupt event i.MX6UL Reference Manual.

http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,572 Views
shammi112
Contributor I

Hi igor,

Can watchdog  wakeup imx6ul from standby/sleep mode ?

Regards,

SHAMMI

0 Kudos
Reply

1,572 Views
igorpadykov
NXP Employee
NXP Employee

yes

Best regards
igor

0 Kudos
Reply

1,572 Views
shammi112
Contributor I

Hi igor,

When device is in standby/deep sleep state , will watchdog  be running ?

My requirement is processor should wakeup every 30 seconds, upon generation of watchdog interrupt.

Regards,

SHAMMI

0 Kudos
Reply

1,572 Views
igorpadykov
NXP Employee
NXP Employee

Hi SHAMMI

watchdog behaviour in low power modes is defined by WDW, WDZST bits in

WDOGx_WCR register.

Best regards
igor

0 Kudos
Reply