Watch dog Reset issue on i.MX 8MQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watch dog Reset issue on i.MX 8MQ

446件の閲覧回数
Manu61
Contributor II

Hi,

We have designed board based on the NXPs i.MX8MQ SoC(Industrial grade), Here we are facing watch dog reset issue.

While running the board or if keep the board in ideal state board is getting reset automatically without any error prints.

When we disable the frequency switching, issue is not there(Fixed to either 800MHz with 0.9V Voltage level or 1.3GHz with 1V Voltage level). When we run the frequency switching only issue is observed. 

I have attached the log.

Best regards,

MK

タグ(1)
0 件の賞賛
返信
1 返信

427件の閲覧回数
Manu61
Contributor II

Hi,

Any update on my above issue ?

Best regards,

MK

0 件の賞賛
返信