Hi,
I'm working on i.MX6Q/Linux platform.
The vpuenc element is built from
L3.0.35_4.1.0_130816/ltib/rpm/BUILD/gst-fsl-plugins-3.0.7/src/video/vpu/src
In my application program, I tried to set the "bitrate" property of "vpuenc" element to 300kbps( 300000bps) but got the following warning msg:
"
GLib-GObject-WARNING **: IA__g_object_set_valist: object class `GstVpuEnc' has no property named ` \xc6\u00'
"
The code snippet is as follows:
static GstElement * create_mfw_vpu_encoder (avsvr_params_t * params)
{
GstElement * encoder = NULL;
uint32_t bitrate = 0, gopsize = 5;
encoder = gst_element_factory_make("vpuenc", "video_encoder");
if (encoder) {
// set encoding quality
if (params->av_params.venc_bitrate > 0)
bitrate = params->av_params.venc_bitrate;
if (params->av_params.venc_gopsize > 0)
gopsize = params->av_params.venc_gopsize;
g_object_set(G_OBJECT(encoder), "bitrate", bitrate, NULL);
g_object_set(G_OBJECT(encoder), "codec", params->av_params.venc_std, NULL);
if(bitrate > 0) { //for CBR encoding, set max_qp and gamma if needed
g_print("CBR encoding!\n");
g_object_set(G_OBJECT(encoder), "bitrate", bitrate, NULL);
}
//gopsize is always set
if(gopsize > 0)
g_object_set(G_OBJECT(encoder), "gopsize", gopsize, NULL);
}
return encoder;
}
Following is my debug procedure and output message:
Breakpoint 1, create_mfw_vpu_encoder (params=0x35f68) at pipeline.c:265
265 GstElement * encoder = NULL;
(gdb) n
266 uint32_t bitrate = 300000, gopsize = 5;
(gdb) n
268 encoder = gst_element_factory_make("vpuenc", "video_encoder");
(gdb) n
269 if (encoder) {
(gdb) n
279 if (params->av_params.venc_bitrate > 0)
(gdb) n
280 bitrate = params->av_params.venc_bitrate;
(gdb) n
282 if (params->av_params.venc_gopsize > 0)
(gdb) p bitrate
$1 = 300
(gdb) n
283 gopsize = params->av_params.venc_gopsize;
(gdb) p gopsize
$2 = 5
(gdb) n
285 g_object_set(G_OBJECT(encoder), "bitrate", bitrate, NULL);
(gdb) n
(gst_svr:2698): GLib-GObject-WARNING **: IA__g_object_set_valist: object class `GstVpuEnc' has no property named ` \xc6\u00'
I'm setting "bitrate" property, why did I get such strange warning message?
And I'm not sure if the "bitrate" property has been correctly set to my desired value or not.
How to check and fix this issue?
BTW, the following command line works well without any problem:
gst-launch -v tvsrc device=/dev/video0 capture-mode=0 ! 'video/x-raw-yuv,format=(fourcc)UYVY,width=720,height=576,framerate=15/1' ! mfw_ipucsc ! 'video/x-raw-yuv,format=(fourcc)I420, width=640,height=480,framerate=15/1' ! vpuenc codec=avc bitrate=300000 gopsize=4 ! video/x-h264,width=640,height=480 ! rtph264pay mtu=1024 ! udpsink host=218.75.199.202 port=5004 sync=false async=false
I can correctly receive and decode the streamed H.264 data on PC receiver.
Any idea?
Robbie