Want to use nodejs 14 from nodejs 10 in yocto warrior bsp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Want to use nodejs 14 from nodejs 10 in yocto warrior bsp

2,615件の閲覧回数
darshakraval
Contributor I

Hi,

I am currently using yocto warrior bsp as my build system for i.mx6ull custom board.

In warrior, nodejs version 10 is running at sources/meta-openembedded/meta-oe/recipes-devtools

I want to use nodejs 14. I couldn't find yocto recipe for nodejs 14.

Is it possible to upgrade from nodejs 10 to nodejs 14 in yocto warrior ?

Thanks in advance.

Darshak

0 件の賞賛
返信
2 返答(返信)

2,443件の閲覧回数
xabiermarquiegu
Contributor II

Hello,

I have backported the required recipes for building nodejs 14.18.1 in Yocto Warrior. Just copy the recipes to your desired layer and give them a try. I know they build, but I haven't been able to test them myself yet. Feel free to contribute if you identify potential improvements:

https://github.com/ainguraXmarquiegui/yocto_nodejs/tree/warrior

0 件の賞賛
返信

2,602件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I didn't try this, but you can download the nodejs 14 and try to install in the warrior bsp, but I'm not sure if the warrior bsp is compatible with nodejs 14, or you can upgrade your bsp to the latest vesrion

 

0 件の賞賛
返信