Want to know the significance of EIM (External Interface Module) in LPDDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Want to know the significance of EIM (External Interface Module) in LPDDR

672 Views
srinivasaporam
Contributor II

Hi,

We are working on the development of a board based on i.MX6 processor. Here we require a board of size 6cmx3cm, that's reason why we are customizing all the components used along with the processor. Now I would like to ask you, what is the significance of EIM module in LPDDR. can I remove this module and if so, will it affect the performance of DDR. Please reply me urgently.

0 Kudos
Reply
1 Reply

594 Views
SergioSolis
NXP Employee
NXP Employee

Hello Srinivasa,

Yes, you can remove it if you are not going to use it, it won't affect LPDDR's performance.


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply