Wandboard stuck in U-Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wandboard stuck in U-Boot

1,781 Views
markbyrnes
Contributor I

After following the instruction in Getting started with Yocto on Wandboard - Wandboard Wiki​  - the Wandboard is stuck in U-Boot.  When building I did deviate from the instructions by using MACHINE=wandboard, but bitbake would not accept "wandboard-solo".  I'm assuming the bootfile is not configured correctly.  Unfortunately I am new to this system - where is the bootfile for the Wandboard located in the Yocto build system?

Has anyone else had this issue? 
Thank you.

below is the console output with boot environmental variables:

U-Boot 2016.03+fslc+gfd6b196 (Mar 27 2016 - 00:23:57 -0700)

CPU:   Freescale i.MX6SOLO rev1.1 at 792 MHz

Reset cause: POR

Board: Wandboard rev C1

I2C:   ready

DRAM:  512 MiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

*** Warning - bad CRC, using default environment

auto-detected panel HDMI

Display: HDMI (1024x768)

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Hit any key to stop autoboot:  0

switch to partitions #0, OK

mmc0 is current device

Scanning mmc 0:1...

MMC: no card present

starting USB...

USB0:   Port not available.

USB1:   USB EHCI 1.00

scanning bus 1 for devices... 1 USB Device(s) found

       scanning usb for storage devices... 0 Storage Device(s) found

USB device 0: unknown device

FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !

BOOTP broadcast 1

...

=> printenv

baudrate=115200

board_name=C1

board_rev=MX6DL

boot_a_script=load ${devtype} ${devnum}:${distro_bootpart} ${scriptaddr} ${pref}

boot_extlinux=sysboot ${devtype} ${devnum}:${distro_bootpart} any ${scriptaddr}f

boot_net_usb_start=usb start

boot_prefixes=/ /boot/

boot_script_dhcp=boot.scr.uimg

boot_scripts=boot.scr.uimg boot.scr

boot_targets=mmc0 mmc1 usb0 pxe dhcp

bootcmd=run findfdt; run distro_bootcmd

bootcmd_dhcp=run boot_net_usb_start; if dhcp ${scriptaddr} ${boot_script_dhcp};i

bootcmd_mmc0=setenv devnum 0; run mmc_boot

bootcmd_mmc1=setenv devnum 1; run mmc_boot

bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi

bootcmd_usb0=setenv devnum 0; run usb_boot

bootdelay=2

bootfstype=fat

console=ttymxc0,115200

devnum=0

devplist=1

devtype=mmc

distro_bootcmd=for target in ${boot_targets}; do run bootcmd_${target}; done

ethact=FEC

ethaddr=00:1f:7b:b0:0c:76

ethprime=FEC

fdt_addr=0x18000000

fdt_addr_r=0x18000000

fdt_high=0xffffffff

fdtfile=imx6dl-wandboard.dtb

findfdt=if test $board_rev = MX6Q ; then setenv fdtfile imx6q-wandboard.dtb; fi

initrd_high=0xffffffff

ip_dyn=yes

kernel_addr_r=0x12000000

loadaddr=0x12000000

mmc_boot=if mmc dev ${devnum}; then setenv devtype mmc; run scan_dev_for_boot_pi

mmcdev=0

pxefile_addr_r=0x12000000

ramdisk_addr_r=0x13000000

ramdiskaddr=0x13000000

scan_dev_for_boot=echo Scanning ${devtype} ${devnum}:${distro_bootpart}..

.; fore
scan_dev_for_boot_part=part list ${devtype} ${devnum} -bootable devplist; env ee
scan_dev_for_extlinux=if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefi
scan_dev_for_scripts=for script in ${boot_scripts}; do if test -e ${devtype} ${e
scriptaddr=0x12000000
splashpos=m,m
update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setei
update_sd_firmware_filename=u-boot.imx
usb_boot=usb start; if usb dev ${devnum}; then setenv devtype usb; run scan_devi
videoargs=setenv nextcon 0; if hdmidet; then setenv bootargs ${bootargs} video=}

Environment size: 3559/8188 bytes

...

0 Kudos
Reply
1 Reply

1,034 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mark

seems uboot-2016 is not integrated yet for this board, as according to

below link latest stable release is uboot-2015.04

wandboard-org · GitHub

one can post on meta-fsl-arm mailing list, so that someone familiar with

that board could try to assist you

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply