Wakeup A core Using GPIO in IMX8ULP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wakeup A core Using GPIO in IMX8ULP

559件の閲覧回数
dhruvinrajpura
Contributor III
Hello,
 
I'm using the i.MX8ULP and have connected two push buttons to PTE11 and PTE14. Now A core is in sleep mode and M core is Running, and I want to wake up the A core when a button is pressed.
 
However, after checking the reference manual, I found that PTE11 and PTE14 are not linked to WUU1. So, is it possible to wake up the A core using these pins? If yes, how can I do that?
 
If not, can I at least get an interrupt on the M core when these buttons are pressed? Is there any way to use these pins on the M core?
 
Thanks!
 
ラベル(1)
0 件の賞賛
返信
0 返答(返信)