Wake-up time for the sleep states

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wake-up time for the sleep states

625 Views
stephane_mouako
Contributor I

I am using the Nitrogen6_MAX equipped with the i.MX6 Quad-Core ARM Cortex-A9 processor which works with the Linux 4.14.0 kernel. According to Linux documentation, the wake-up time for supend-to-s2idle is less than the wake-up time for Suspend-to-RAM. But I measured these wake-up times with Oszilloscop and I noticed that the wake-up time of supend-to-s2idle is greater than the wake-up time for Suspend_to_RAM. Can someone please explain this to me?

0 Kudos
1 Reply

564 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mouako

wake time additionally depends on used software, as described below

pastedImage_2.jpg

since Nitrogen6_MAX board and its software was developed by boundary devices, issue

may be posted on its support: https://boundarydevices.com/wiki-bd/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos