Hi, i have the following problem with iMX8MPlus
when I put the system in sleep
echo mem > /sys/power/state
I am able to wake up the system with the touchscreen interrupt but only when the core M7 is not running.
If the M7 runs, with my application, the system doesn't woke up.
The touch interrupt is in exclusive use of A53
Hello,
when M7 is running the touch works correctly, the touch is on
 AldoG
		
			AldoG
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
Apologize for the delayed response, as stated in the App note this is actually possible but it is not possible by default, please refer to the chapter 4.3 Make the M core alive when the A core is in Suspend mode for more information.
Going back to the issue at hand, are you using an NXP EVK, right?
Could you share the device tree that you are using?
Best regards/Saludos,
Aldo.
 AldoG
		
			AldoG
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
When you have M7 running, does the touch work correctly?
Is the M7 running or in sleep as well?
Also, how are your touch connected? is it I2C?
To which port is connected?
Best regards/Saludos,
Aldo.