WMV (Windows Media) codecs for i.MX53?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WMV (Windows Media) codecs for i.MX53?

1,918 Views
sidebranch
Contributor II

Hello,

further enhancing my build, I could not find any support for WMF (Windows Media Format) decoders in /fsl-mm-codeclib-2.0.3/release/lib/

Also, my gst-fsl-plugins fail to build the corresponding wmv plugins.

configure: *** checking feature: WMV9MP_DEC library ***
configure: *** for plug-ins: WMV9MP_DEC plugin ***
checking wmv9mp_dec_api.h usability... no
checking wmv9mp_dec_api.h presence... no
checking for wmv9mp_dec_api.h... no
configure: *** These plugins will not be built: WMV9MP_DEC plugin

configure: *** checking feature: WMV78_DEC library ***
configure: *** for plug-ins: WMV78_DEC plugin ***
checking wmv789_dec_api.h usability... no
checking wmv789_dec_api.h presence... no
checking for wmv789_dec_api.h... no
configure: *** These plugins will not be built: WMV78_DEC plugin

However, in the Ubuntu image, these GST plugins are present:

lucid@lucid-desktop:/usr/lib$ find | grep wmv
./gstreamer-0.10/libmfw_gst_wmvdec.so
./gstreamer-0.10/libmfw_gst_wmv9mpdec.so

Where can I find the wmv support?

Thanks,

Leon.

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

1,669 Views
sidebranch
Contributor II

Thanks for the answer.

0 Kudos
Reply

1,669 Views
KanHU
Contributor III

the  wmv support is not included in the standard codec release. You need license to get those sort of codecs.

0 Kudos
Reply

1,669 Views
sidebranch
Contributor II

Hello all,

More specifically, I would like to obtain/build these codecs files:

fsl-mm-ms-codeclib-2.0.3.tar.gz

From the LTIB log:

Try fsl-mm-ms-codeclib-2.0.3.tar.gz.md5 from the GPP http://bitshrine.org/gpp/fsl-mm-ms-codeclib-2.0.3.tar.gz.md5: 22:12:18 ERROR 404: Not Found. Try fsl-mm-ms-codeclib-2.0.3.tar.gz from the GPP http://bitshrine.org/gpp/fsl-mm-ms-codeclib-2.0.3.tar.gz: 22:12:19 ERROR 404: Not Found. Can't get: fsl-mm-ms-codeclib-2.0.3.tar.gz at ./ltib line 790.

Thanks for any help,

Leon Woestenberg.

0 Kudos
Reply

1,669 Views
sidebranch
Contributor II

Where can I find the WMV support? I cannot find these in the LTIB package when building my own rootfs.

0 Kudos
Reply