Hi.
I have an imx6qp saber board and I am testing android 9.0.
I also want to use the murata type 1dx module.
Download P9.0.0_2.2.0 ga demo image and download type 1dx firmware.
I copied it to the / vendor / firmware / brcm folder.
However, the wifi module is not recognized.
Module wlreg on pin does not become "Active High".
I have checked with P9.0.0_2.3.4 android souce.
There are no imx6qp-sabresd-btwifi.dts and imx6qdl-sabresd-btwifi.dtsi files in the "Android_build / vendor / nxp-opensource / uboot-imx / arch / arm / dts" folder.
The contents of the file can be checked at the link below.
https://android.googlesource.com/platform/hardware/bsp/kernel/freescale/+/master/arch/arm/boot/dts/i...
Does Murata WiFi module not support?
Please let me know how I can do it.
Hello An jin ho,
By default, i.MX6QP SabreSD board doesn't support the WIFI, But you can port it to your own board based on i.MX6QP, some customers are using the WIFI module.
See the link, please!
WiFi (Murata chip) is not working on i.MX6Q board
In addition, on our sabreSD board, Murata wifi is used , whose part number is LBEH5HMZPC-TEMP, you can find it on schematic.
I checked the WIFI modue you want on MuRata website:
If you search CYW4343W on our community, you can find some solutions on it.
Hope above information is helpful to you.
Have a nice day!
B.R,
Weidong