WLAN & WAP configuration in Yocto on i.MX8 without reboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WLAN & WAP configuration in Yocto on i.MX8 without reboot

2,737 Views
srikanth_vemula
Contributor II

Hi,

We are working on yocto build on the i.MX8 platform. We've a requirement to set up the below mentioned parameters (without system reboot) based on user's selection, through GUI, for WLAN & WAP configuration:

1. WAP configuration :

setting SSID, SSID broadcast enable/disable, Key,  Security Protocol etc.

I could find the file for WAP configuration : 

/etc/wpa_supplicant/wpa_supplicant-wlan0.conf

But looks like it doesn't have option for controlling SSID broadcast enable/disable. 

2. WLAN configuration:

Setting Host name, Domain Name, Gateway/IP Mask, Enable/Disable DHCP, DNS blocks etc.

To my knowledge, the file /etc/network/interfaces can be used to configure the IP address, gateway etc, but I could not find any configuration file for the above parameters.

Requesting your suggestions please... 

Regards,

Srikanth Vemula.

0 Kudos
Reply
4 Replies

2,607 Views
johnnosky
Contributor I

Hi srikanth_vemula,

Apologies for the late reply on this thread, it was only recently made aware to us on the support team at Laird Connectivity.

We provide an external layer for building our firmware, driver, supplicant and NetworkManager into your Yocto image. Please find our GitHub repo in the following link:

https://github.com/LairdCP/meta-laird-cp

If support is needed, please contact us through our support portal (click "Open a Support Ticket" at the bottom):

https://www.lairdconnect.com/resources/support

0 Kudos
Reply

2,686 Views
srikanth_vemula
Contributor II

Hi,

I missed to mention the wi-fi module. We're using Laird 60-2230C based WiFi solution. Can you please provide whether NXP has any yocto layer for Laird also, So that it would be useful for me to address my requirement. and also request you to provide sample configuration files for configuring the aforementioned parameters.

Regards,

Srikanth Vemula.

0 Kudos
Reply

2,686 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srikanth

I am afraid Laird modules are not supported, supported models are given on

above link, also one can look at Linux Manual WiFi Chapter included in documentation packages on

Embedded Linux for i.MX Applications Processors | NXP 

For Laird modules sample configuration files suggest to apply to vendor of these modules directly.

Best regards
igor

0 Kudos
Reply

2,686 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srikanth 

one can look at latest wifi linux manual on

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply