WLAN,BT and GPS disable in Android Build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WLAN,BT and GPS disable in Android Build

ソリューションへジャンプ
1,979件の閲覧回数
anjojohn
Contributor IV

Hi all, 

i have a custom board with IMX6 based on sabresd. for reducing memory footprint , i would like to disable wlan, bt and gps module from building. Any help is appreciated

1 解決策
1,875件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi anjo

one can look at Linux Manual included in Linux L4.14.98_2.0.0 Documentation

and disable appropriate drivers using section "Menu Configuration Options" Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,876件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi anjo

one can look at Linux Manual included in Linux L4.14.98_2.0.0 Documentation

and disable appropriate drivers using section "Menu Configuration Options" Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------