WIFI SDIO SDK and related net documents

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

WIFI SDIO SDK and related net documents

跳至解决方案
4,959 次查看
JustinWu2
Contributor III

Dear ALL:

Do you have the Atheros 6K SDK and porting guide for i.MX6Q? I want to reference it's SDIO Wifi design. Do you have Broadcom WL-211 (BCM-40181)or WL-212 Wifi porting guide for freescale i.MX6Q?

Where can I get the Atheros 6103 SDK and related documents? I study the Android Advanced User Guide and find WIFI brief. Where can I study and get the further integration between i.MX6Q and SDIO WIFI? Whether does Someone use broadcom ,Realtek, or Ralink sdio wifi which is integrated with i.MX6Q net documents?

Best Regards,

Justin Wu

0 项奖励
回复
1 解答
2,521 次查看
JustinWu2
Contributor III

The 6103 and 6003 firmware.

You can git the following source.

linux/kernel/git/firmware/linux-firmware.git - Repository of firmware blobs for use with the Linux kernel

Atheros AR6003 SDIO WiFi Integration

https://developer.ridgerun.com/wiki/index.php/Atheros_AR6003_SDIO_WiFi_Integration

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,521 次查看
JustinWu2
Contributor III

Dear all:

I find the following information.

Support RTL8188 8192 wifi dongle in FSL JB4.2.2-GA release


https://community.freescale.com/docs/DOC-94880


Provide WiFi support on Android ICS with iMx6Q board.

https://community.freescale.com/message/307928#307928


Driver for Texas Instruments' Wilink(tm) combo devices WL1271/3 and WL1281/3
http://wireless.kernel.org/en/users/Drivers/wl12xx


Marvel WLAN, SDIO, Linux and imx53


https://community.freescale.com/message/317897#317897


Porting SD8686 WIFI Drivers to Android

https://code.google.com/p/km233/wiki/WIFI_TO_ANDROID

Best Regards,

Justin Wu

2,522 次查看
JustinWu2
Contributor III

The 6103 and 6003 firmware.

You can git the following source.

linux/kernel/git/firmware/linux-firmware.git - Repository of firmware blobs for use with the Linux kernel

Atheros AR6003 SDIO WiFi Integration

https://developer.ridgerun.com/wiki/index.php/Atheros_AR6003_SDIO_WiFi_Integration

0 项奖励
回复