WFD Sink with non-Google (Nexus) devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WFD Sink with non-Google (Nexus) devices

861 Views
YongJunChang
Contributor II

Hi all,

We are developing a system which has Miracast functionality in i.MX6 platform.

Thanks to the Freescale's libfsl_wfd.so, we are able to connect all Nexus devices as a WFD source.

FYI, our system runs as a WFD sink.

But when I try to connect to our MX6 device from non-Google devices such as Galaxy S3/S4, I got the following messages;

E/WifiDisplaySink( 1478): Invalid server_port description '19000'.

F/WifiDisplaySink( 1478): frameworks/imx-wfd/jni/sink/WifiDisplaySink.cpp:508 CHECK_EQ( err,(status_t)OK) failed: -1007 vs. 0

F/libc    ( 1478): Fatal signal 11 (SIGSEGV) at 0xdeadbaad (code=1), thread 2463 (ALooper)

Do you have any ideas to use non-Google devices?

Thanks in advance!

Labels (4)
0 Kudos
1 Reply

359 Views
saurabh206
Senior Contributor III

Hi,

Yong

Which Wi-FI module are you using?

0 Kudos