WEC7, imx53, HIVE Registry store on the SD card, but cannot modify it

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WEC7, imx53, HIVE Registry store on the SD card, but cannot modify it

3,803件の閲覧回数
wangyx
Contributor III

Dear all

 

     My board is imx.53 SMD,I want to store my registry on the 8G SD card.

     Now encountered three problems:

     1.    The HIVE registry can not be modified.  I write a key , and refresh, returns an error value of 23.

               Also the SD card can not create a new folder .

     2.     Sometimes when I refresh my SD card , the folder is hidden , but can access

     3.    I set the registry path '\Registry\system.hv', but at the same time another folder (windows) is created

 

    Please help me, thx~

Original Attachment has been moved to: esdhc_mx53.reg.zip

Original Attachment has been moved to: platform.reg.zip

ラベル(1)
タグ(2)
0 件の賞賛
返信
5 返答(返信)

2,416件の閲覧回数
AlexeyT
Contributor III

Hello,

Does your CE kernel image include LAN driver for FEC?

If so I would recommed you to have a look at my question (see below).

WinEC7 - full LAN (FEC) driver disrupts SDHC driver operation if started after SDHC driver

I saw such a behaviour you just described.

When I tried to instantiate FEC NDIS driver after SDHC card driver it caused SD card driver to malfunction and I saw exactly the same thing: SD card folder was visible but attempt to write to it was usually causing error 23 (sometimes error 19).

Placing registry on SD card required SD card driver to load BEFORE FEC LAN driver

Try removing FEC support from OS design and check whether it make any difference or not.

Best regards

0 件の賞賛
返信

2,416件の閲覧回数
seetha
Contributor III

No Alexey,

I have not faced this issue and I have not implemented this feature of FEC

0 件の賞賛
返信

2,416件の閲覧回数
admin
Specialist II

Deactivated user, can you help with this WEC7 question?

0 件の賞賛
返信

2,416件の閲覧回数
wangyx
Contributor III

No people? The Freescale engineer or of other colleagues, Please. Thx~~~~~~~

0 件の賞賛
返信

2,419件の閲覧回数
admin
Specialist II

Any ideas on this, Deactivated user?  Thanks.

0 件の賞賛
返信