WEC7, imx53, HIVE Registry store on the SD card, but cannot modify it

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WEC7, imx53, HIVE Registry store on the SD card, but cannot modify it

3,953 Views
wangyx
Contributor III

Dear all

 

     My board is imx.53 SMD,I want to store my registry on the 8G SD card.

     Now encountered three problems:

     1.    The HIVE registry can not be modified.  I write a key , and refresh, returns an error value of 23.

               Also the SD card can not create a new folder .

     2.     Sometimes when I refresh my SD card , the folder is hidden , but can access

     3.    I set the registry path '\Registry\system.hv', but at the same time another folder (windows) is created

 

    Please help me, thx~

Original Attachment has been moved to: esdhc_mx53.reg.zip

Original Attachment has been moved to: platform.reg.zip

Labels (1)
Tags (2)
0 Kudos
Reply
5 Replies

2,566 Views
AlexeyT
Contributor III

Hello,

Does your CE kernel image include LAN driver for FEC?

If so I would recommed you to have a look at my question (see below).

WinEC7 - full LAN (FEC) driver disrupts SDHC driver operation if started after SDHC driver

I saw such a behaviour you just described.

When I tried to instantiate FEC NDIS driver after SDHC card driver it caused SD card driver to malfunction and I saw exactly the same thing: SD card folder was visible but attempt to write to it was usually causing error 23 (sometimes error 19).

Placing registry on SD card required SD card driver to load BEFORE FEC LAN driver

Try removing FEC support from OS design and check whether it make any difference or not.

Best regards

0 Kudos
Reply

2,566 Views
seetha
Contributor III

No Alexey,

I have not faced this issue and I have not implemented this feature of FEC

0 Kudos
Reply

2,566 Views
admin
Specialist II

Deactivated user, can you help with this WEC7 question?

0 Kudos
Reply

2,566 Views
wangyx
Contributor III

No people? The Freescale engineer or of other colleagues, Please. Thx~~~~~~~

0 Kudos
Reply

2,569 Views
admin
Specialist II

Any ideas on this, Deactivated user?  Thanks.

0 Kudos
Reply