Hi,
working with WEC2013 BSP v2.4 for iMx6 from Adeneo, I've found an error build OS during VPU.DLL build:
BUILD: [00:0000001903:PROGC ] Analyzing project dependency information for pass EXPLIB.
BUILD: [00:0000002059:PROGC ] Building EXPLIB Pass in C:\wince800\platform\iMX6Q_SABRE_Lite\src\drivers\vpu\ directory.
BUILD: [01:0000002106:PROGC ] Linking C:\WINCE800\osdesigns\iMX6Q_SABRE_Lite\Wince800\iMX6Q_SABRE_Lite_ARMV7_Retail\cesysgen\platform\iMX6Q_SABRE_Lite\lib\ARMV7\retail\vpu.lib
BUILD: [01:0000002122:PROGC ] Error(s) in directory "C:\wince800\platform\iMX6Q_SABRE_Lite\src\drivers\vpu\".
BUILD: [01:0000002122:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_Close {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(42)"}
BUILD: [01:0000002137:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_Deinit {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(43)"}
BUILD: [01:0000002137:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_IOControl {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(44)"}
BUILD: [01:0000002137:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_Init {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(45)"}
BUILD: [01:0000002137:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_Open {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(46)"}
BUILD: [01:0000002137:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_PowerDown {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(47)"}
BUILD: [01:0000002137:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_PowerUp {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(48)"}
BUILD: [01:0000002137:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_Read {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(49)"}
BUILD: [01:0000002137:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_Seek {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(50)"}
BUILD: [01:0000002137:ERRORE] vpu.def : error LNK2001: unresolved external symbol VPU_Write {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(51)"}
BUILD: [01:0000002137:ERRORE] C:\WINCE800\osdesigns\iMX6Q_SABRE_Lite\Wince800\iMX6Q_SABRE_Lite_ARMV7_Retail\cesysgen\platform\iMX6Q_SABRE_Lite\lib\ARMV7\retail\vpu.lib : fatal error LNK1120: 10 unresolved externals {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(52)"}
BUILD: [01:0000002168:ERRORE] NMAKE : fatal error U1077: 'C:\WINCE800\sdk\bin\i386\ARM\link.exe' : return code '0x460' {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(53)"}
BUILD: [01:0000002168:ERRORE] TargetExpLibFiles -nologo BUILDMSG=Stop. BUILDROOT=C:\WINCE800\platform\iMX6Q_SABRE_Lite CLEANBUILD=1 LINKONLY=1 NOPASS0=1 failed - rc = 2 {log="C:\WINCE800\platform\iMX6Q_SABRE_Lite\SRC\DRIVERS\VPU\bldsys.log(54)"}
I've verified that, differently from WEC7 BSP, 'vpu_mx6q_fsl_v4.lib' present on ..\platform\common\src\soc\MX6Q_FSL_V4\VPU\LIB\ARMV7\RETAIL\800 folder and that will be linked in 'vpu.dll', doesn't contain function definitons the generate "unresolved external symbol" errors.
'vpu_mx6q_fsl_v4.lib' is released as binary without source code (so it seems).
How can I link VPU.DLL library?
Thanks in advance.
Sorry for the delay in responding, but I have not had the opportunity to work up till now.
I created a new virtual machine with a clean install of windows 8 and WEC2103 with Visual Studio 2012 without updates.
With the BSP I find the same error in compilation when I add the component VPU.
I suppose that the problem could be in 'vpu_mx6q_fsl_v4.lib' library that doesn't contain the functions defined in vpu.def
hello every one,could you help download the source BSP on IMX6D/Q,
THE BSP IS iMX6Q_SABRE_Lite_WEC2013_3.1.1.5-2014-06-13.zip or others version ;
sent a link to my email enjin,sun@flextronics.com TKS!!!
Hello AdeneoEmbedded , are you able to help with this question?
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.
For details please see general advice Where to post a Discussion?
Thank you for using Freescale Community.