WEC2013 BSP on i.MX6 platforms comes with only WEC7 binaries for GPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WEC2013 BSP on i.MX6 platforms comes with only WEC7 binaries for GPU

1,222 Views
christianschmid
Contributor I

Hello everybody.

I'm working on the SabreLite platform with brandnew WEC2013 BSP.

Unfortunately I realized that all included GPU binary DLLs are built for WEC7 (THUMB) although two different folders for 700 and 800 exist.

(Same applies for FILES content)

The files in folders "700" and "800" are binary identical.

Kernel in WEC2013 is compiled for ARMv7 with THUMB2 instructions (only).

So I get the error message "Cannot load executable built for os version 7.00" when I try to start "cube.exe" for instance.

Does anybody know whether GPU binaries compiled for THUMB2 will be released in future BSP versions?

I want to test the OpenGL/OpenVG capabilities with WEC2013.

Thanks a lot.

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

605 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Deactivated user can you  help on this case?

0 Kudos
Reply