Hello everybody.
I'm working on the SabreLite platform with brandnew WEC2013 BSP.
Unfortunately I realized that all included GPU binary DLLs are built for WEC7 (THUMB) although two different folders for 700 and 800 exist.
(Same applies for FILES content)
The files in folders "700" and "800" are binary identical.
Kernel in WEC2013 is compiled for ARMv7 with THUMB2 instructions (only).
So I get the error message "Cannot load executable built for os version 7.00" when I try to start "cube.exe" for instance.
Does anybody know whether GPU binaries compiled for THUMB2 will be released in future BSP versions?
I want to test the OpenGL/OpenVG capabilities with WEC2013.
Thanks a lot.
Deactivated user can you help on this case?