Vsync interrupt at 120fps for i.mx8 mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vsync interrupt at 120fps for i.mx8 mini

673 Views
kailas_kharse
Contributor IV

Hello,

I want to know that currently, MIPI-DSI is supporting 1920x1080 with 60fps for i.Mx8 Mini, but if we reduce the resolution to 960x320, then does imx8 mm supports 120fps?"

Also, with video playback with generating vsync interrupt at 120fps?

 

Thanks & Regards,

Kailas Kharse

Labels (1)
Tags (1)
0 Kudos
3 Replies

669 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kailas

 

> if we reduce the resolution to 960x320, then does imx8 mm supports 120fps?"

 

yes this can be achieved

 

> with video playback with generating vsync interrupt at 120fps?

 

yes

 

Best regards
igor

 

 

 

0 Kudos

663 Views
kailas_kharse
Contributor IV

Hello Igor,

 

Thank you for your quick response.

I wanted to create two frame buffers and use them on a single display, but the buffer shall switch at each Vsync interrupt.

How Can I achieve the above? Where are the changes that need to be done to achieve this?

 

Thanks & Regards,
Kailas Kharse

 

Tags (1)
0 Kudos

660 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kailas

 

for such specific customer tasks NXP has special support service :

https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

0 Kudos