Voltage on SNVS Supply

cancel
Showing results for 
Search instead for 
Did you mean: 

Voltage on SNVS Supply

506 Views
sadatanvashisth
Contributor II

I am using IMX6ul processor with PMIC PF3000A3. We are facing below mentioned issue:

1. There is no supply available for processor including VDD_SNVS_IN.

2. There is a pull up (from an always ON supply) connected on a SNVS powered pin.

3. With out powering up the processor we are getting 2.6V on VDD_SNVS_IN .

In this case if I connect a always ON supply to VDD_SNVS_IN , then we are not able to turn the processor ON once the processor goes into power off until we remove power from VDD_SNVS_IN as well.

Some one please suggest what could be the possible cause of this issue and how we should solve this.

Regards,

Sadatan

Labels (1)
0 Kudos
1 Reply

341 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Sadatan

this may be board layout errors, one can try to make board

with minimal components soldered and check VDD_SNVS.

There are recommendations given in Chapter 4 Avoiding Board Bring-up Problems

Hardware Development Guide for the i.MX 6UltraLite Applications Processor

which may be useful to trace them.
http://www.nxp.com/docs/en/user-guide/IMX6ULHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos