Voltage level of power-up sequence i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voltage level of power-up sequence i.MX6ULL

907 Views
ban45
Contributor III

Hi

Power-on sequence Is it okay to input a voltage below the input voltage range level of the power port before the sequence?

There is a power supply pin with a voltage of 1V or less, so I would like to check if there is a problem without taking any measures.

 

best regard

0 Kudos
Reply
1 Reply

888 Views
b36401
NXP Employee
NXP Employee

It is not allowed to have a voltage.
Accrodingly to Power-Up Sequence described in the DataSheet VDD_SNVS_IN supply must be turned on before any other power supply.

0 Kudos
Reply