Voltage difference between VDD_ARM_CAP and VDD_SOC_IN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voltage difference between VDD_ARM_CAP and VDD_SOC_IN

Jump to solution
1,110 Views
kladu
Contributor II

Hi,

we are using i.MX6ULL with fixed power supplies (not PMIC). Datasheet (Table 10, Page 24) claims that VDD_SOC_IN MUST be 125 mV higher than the LDO Outputs.

Difference between VDD_SOC_IN and VDD_ARM/SOC_CAP at upper voltage limit (1.5V vs 1.26V) is larger than 125mV.

Should this difference be understood as exactly 125mV or at least 125mV? If it is exactly, what is the tolerance and how to deal with upper voltage level mismatch?

Thanks,
kladu

Screenshot 2022-01-06 at Thu, 6 Jan, 12.47.23 PM.png

 

Labels (1)
0 Kudos
1 Solution
1,103 Views
igorpadykov
NXP Employee
NXP Employee

Hi Borut 

 

>Should this difference be understood as exactly 125mV or at least 125mV?

 

yes it should be at least 125mV, sorry for confusion.

 

Best regards
igor

View solution in original post

2 Replies
1,099 Views
kladu
Contributor II

That's what I thought, thanks Igor.

0 Kudos
1,104 Views
igorpadykov
NXP Employee
NXP Employee

Hi Borut 

 

>Should this difference be understood as exactly 125mV or at least 125mV?

 

yes it should be at least 125mV, sorry for confusion.

 

Best regards
igor