Voltage Level of USB1_ID and USB2_ID of i.MX 8M Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voltage Level of USB1_ID and USB2_ID of i.MX 8M Mini

714 Views
peterlischer
Senior Contributor I

What are the voltage levels of the dedicated USB1_ID and USB2_ID pins of the i.MX 8M Mini? I was not able to find any electrical information about these pins in the datasheet or the hardware design guide. Are these pins 1.8V logic level or 3.3V? Is there any internal pull-up or pull-down resistor?

Labels (1)
0 Kudos
1 Reply

587 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  According to table "i.MX 8M Mini 14 x 14 mm functional contact assignments" in i.MX 8Mm Datasheet,

USB1_ID  and USB2_ID are powered by VDD_USB_1P8 (1.8V)

  

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos