What are the voltage levels of the dedicated USB1_ID and USB2_ID pins of the i.MX 8M Mini? I was not able to find any electrical information about these pins in the datasheet or the hardware design guide. Are these pins 1.8V logic level or 3.3V? Is there any internal pull-up or pull-down resistor?
Hello,
According to table "i.MX 8M Mini 14 x 14 mm functional contact assignments" in i.MX 8Mm Datasheet,
USB1_ID and USB2_ID are powered by VDD_USB_1P8 (1.8V)
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.