Voip Based Chip on Baremetal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Voip Based Chip on Baremetal

1,304件の閲覧回数
rama_krishna
Contributor II

Dear All,

               We are looking for SOC for using in Voip Application. The SOC should work Baremetal Software(No OS). The SDK should include SIP Protocol stack. Please suggest some SOC's and SDK's Available.

Thanks & Regards

Rama Krishna

1 返信

977件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Rama,

In case of the i.MX6 series of applications processors, you could refer to the “i.MX 6Series Platform SDK”, a bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for many peripherals, and much example code.

Other option (depending of the required performance) could be a Kinetis MCU, running MQX RTOS, or if you are really looking for a bare-metal option, you could refer to fNET at these links:

http://fnet.sourceforge.net/

https://community.freescale.com/message/81528

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------