Voice Recognition Solution with Echo Cancellation and Noise Reduction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voice Recognition Solution with Echo Cancellation and Noise Reduction

1,141 Views
JK_Cha
Contributor IV

Hi NXP.

Please recommend a solution in the iMX 8M/9 series for voice recognition and noise reduction or cancellation. It is difficult to check the external audio codec in the reference, so is it possible to implement functions such as voice recognition and noise removal with 8MP or 9 series of built-in NPU?
 
Application is Smart Intercom based on i.MX 8MP or 95 device. Firstly customer would like to begin development with 8MP for now.
 
Regards, 
ADAM
0 Kudos
Reply
5 Replies

1,068 Views
JK_Cha
Contributor IV

Hi Sanket

The link can not be accessible by me. 

Please give me the material if possible.

Thanks.

Regards, 

Jack

 

You do not have sufficient privileges for this resource or its parent to perform this action.

Click your browser's Back button to continue.

 
0 Kudos
Reply

1,043 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @JK_Cha ,

I hope you are doing well.

Please confirm do you have NDA signed, If yes please share your NDA number.
So that we can verify the same and share the information with you.

Thanks & Regards,
Sanket Parekh

0 Kudos
Reply

1,087 Views
JK_Cha
Contributor IV

Hi Sanket.

Thanks for your kind answer.

 

Can you please also recommend about Echo Cancellation on 8MP and 95?

The customer firstly look into 8MP, then move to 95 later.

8MP seems have internal DSP. But 95 does not. The application is Doorlock Intercom based on MPU.

Thanks.

Regards, 

ADAM

0 Kudos
Reply

1,073 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @JK_Cha ,

I hope you are doing well,

->As of now there are no other references available for imx93 & imx8mp for echo cancellation.
Because imx93 is in the pre-production stage.

One can refer to this link for reference only.
https://community.nxp.com/t5/Block-Diagrams-Knowledge-Base/BD-Echo-Cancellation-and-Noise-Reduction/...

I hope it helps!

Thanks & Regards,
Sanket Parekh

0 Kudos
Reply

1,110 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @JK_Cha ,

I hope you are doing well.

->i.MX 8M family are supported platform by Voice Enablement Software for Application processors.
I have shared the link of Voice-Enablement-Software-Six-Pack for your reference, Please find it from the below link.
https://community.nxp.com/t5/i-MX-Processors/Voice-Recognition-solution-of-i-MX-8X-family/td-p/14929...

I hope this helps!

Thanks & Regards,
Sanket Parekh