Hi all,
The Vivante GPU driver fails to initialize on a system with 4GB DDR. It prints a "AXI BUS ERROR" line in the kernel messages and then prints a number of various register/memory dumps.
The driver works normally on the same system if DDR size is limited to 3GB with the "mem=3072MiB" kernel parameter.
It is a known issue? Is there a fix/workaround?
Regards,
Dmitry
vivante
Hello,
It is a known issue that GPU driver doesn't support 4GB memory address range in GA release.
Now NXP is working to fix this issue. Please create request / ticket for more details.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!