Violet screen when using iMX6S + TP2854 + Camera HDTVI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Violet screen when using iMX6S + TP2854 + Camera HDTVI

964 次查看
toanjunifer
Senior Contributor I

Hi,

I'm trying to use Camera HDTVI with TP2854 in iMX6S(Linux 4.1.15). After try some example program in unit_test folder, such as: 

   $ ./mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 & sleep 10

I get only violet screen:

violet.jpeg

Someone can tell me why does it happened ? And how to fix it ?

Thank you so much,

Toan

标签 (1)
3 回复数

854 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dao

one can look at below link:

iMX6DQ TP2854 MIPI CSI2 720P HD-TVI camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

854 次查看
toanjunifer
Senior Contributor I

Thank you igorpadykov‌, I read this article before but it does solve my problem. Do you have any suggestions ? 

Thanks in advance,

Toan

0 项奖励

854 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dao

 

one can debug it running in parallel this demo and custom board and

comparing ipu registers, use as additional help

Using Open Source Debugging Tools for Linux on i.MX Processors

 

Best regards
igor