Video playback issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Video playback issues

1,016 次查看
IanCraig
Contributor II

Hi

I wonder if anyone can help with a couple of video playback issues.

My setup is a core-image-sato build with gstreamer and chromium using the "Fido" branch of the fsl-community-bsp and I am playing a H.264 video file.

1. Using the media player playback is good but if I put the display in to portrait mode using "xrandr" playback of the same video file is not good. CPU usage for gtk-play goes from 12% to 40%. Does anyone know if there are issues with hardware acceleration in portrait mode or a way to fix this.

2. I've built chromium but I can't play any H.264 files at all. Does anyone know if chromium can play these files or how I go about getting them to play.

Thanks

Ian

0 项奖励
回复
1 回复

881 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ian,

Current xrand is supported however there are some features that are not accelerated by GPU, and this is marked as a bug.

Reduced graphic performance with rotated screen (imx6, sabresd)

Hope this helps

0 项奖励
回复