Hello,
I have a custom board based on the i.MX8M platform - I am not able to play the following two video format files:
1. .mkv video with VP8 decoder
2. .wmv video with a VC1 decoder.
The following VPUs are enabled in my kernel configuration:
CONFIG_MXC_HANTRO=y
CONFIG_MXC_HANTRO_845=y
CONFIG_MXC_HANTRO_845_H1=y
CONFIG_MXC_VPU_MALONE=y
CONFIG_MXC_VPU_WINDSOR=y
The command used to play the video is:
gst-launch-1.0 filesrc location=<Path to Video file>.wmv typefind=true ! video/quicktime ! qtdemux ! queue max-size-time=0 ! vpudec ! queue max-size-time=0 ! waylandsink
Are we missing any additional configurations/steps to support the playback of these file formats?
Any insight on the issue would help!