Version of the Vivante GPU driver in i.MX6 3.14.28-1.0.0-ga Linux BSP release

cancel
Showing results for 
Search instead for 
Did you mean: 

Version of the Vivante GPU driver in i.MX6 3.14.28-1.0.0-ga Linux BSP release

1,307 Views
carstenkrueger
Contributor I

The release notes for 3.14.28-1.0.0-ga state that there is a new version of the Vivante GPU driver included (v5.0.11p4.4).

However when looking at the driver in git here http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/drivers/mxc/gpu-viv/hal/kernel/ inc/gc_hal_version.h?h=imx_3.14.28_1.0.0_ga

there seems to be no change compared to what was released in 3.10.53_1.1.0-ga (v5.0.11p4.1 according to the release notes).

Am I overlooking something?

Labels (3)
0 Kudos
1 Reply

115 Views
joanxie
NXP TechSupport
NXP TechSupport

compare to the two driver, it seems they don't have big change between them.

0 Kudos