Vbus detection issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vbus detection issue

1,081件の閲覧回数
asmaa
Contributor V

Hello All,

On our custom board based on imx6ul, We are trying to use USB for charger detection. In device driver it is giving me following error "vbus not valid". My device tree seem to be correct shown as below:

&usbotg1 {
pinctrl-names = "default";
dr_mode = "peripheral";
imx6-usb-charger-detection;
srp-disable;
hnp-disable;
adp-disable;
status = "okay";
};

As suggested in charger algorithm of IMX6ULRM,  ENABLE_ILIMIT and ENABLE_LINREG is enabled and also VBUSVALID_THRESH is set to 4.4V. I measured VBUS volatage it is coming out to 4.93V.

Can someone at NXP, please help to understand what are the other parameters I need to consider?

Regards,

Asma

0 件の賞賛
返信
1 返信

1,013件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,


Could you provide an schematic for this custom board (USB part)?

 

Thank you,

Regards,

Aldo.

0 件の賞賛
返信