Hi, I am reading the document i.MX 6 Linux High Assurance Boot (HAB) User's Guide, Rev. L3.0.35_1.1.0, 01/2013 which mentions how to use the HAB on the i.MX6 to validate uImages.
I have been trying the feature with some success. Some notes:
These are my results:
This behaviour I find confusing:
This is the complete output:
U-Boot dub-2015.04-r4+gef02d8ca6e65 (Jun 08 2016 - 10:49:38)
CPU: Freescale i.MX6Q rev1.5 1200 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 44C
Reset cause: POR
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0 (eMMC), FSL_SDHC: 1
In: serial
Out: serial
Err: serial
Boot device: MMC4
PMIC: DA9063, Device: 0x61, Variant: 0x50, Customer: 0x00, Config: 0x56
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
reading boot.scr
2042 bytes read in 19 ms (104.5 KiB/s)
## Executing script at 12000000
reading uImage
5001248 bytes read in 155 ms (30.8 MiB/s)
reading uImage-imx6q-ccimx6sbc-wb.dtb
45292 bytes read in 22 ms (2 MiB/s)
Authenticate image from DDR location 0x12000000...
hab_rvt_entry success :smileyhappy:
ivt_offset = 0x4c3000, ivt addr = 0x124c3000
Dumping IVT
124c3000: 402000d1 12001000 00000000 00000000 .. @............
124c3010: 00000000 124c3000 124c3020 00000000 .....0L. 0L.....
Dumping CSF Header
124c3020: 405000d4 000c00be 00001703 50000000 ..P@...........P
124c3030: 020c00be 01000009 90040000 000c00ca ................
124c3040: 0000c501 e4070000 000c00be 02000009 ................
124c3050: e8090000 001400ca 0000c502 3c0d0000 ...............<
--- Status before ---
Secure boot disabled
HAB Configuration: 0xf0, HAB State: 0x66
No HAB Events Found!
--- ------------- ----
Calling authenticate_image in ROM
ivt_offset = 0x4c3000
start = 0x12000000
bytes = 0x4c5020
load_addr: 301993984
hab_rvt_exit() success :smileyhappy:
--- status after ---
Secure boot disabled
HAB Configuration: 0xf0, HAB State: 0x66
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0f 0xc0 0x00
0xbe 0x00 0x0c 0x00 0x03 0x17 0x00 0x00
0x00 0x00 0x00 0x50
--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x12 0x4c 0x30 0x00
0x00 0x00 0x00 0x20
--------- HAB Event 3 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x12 0x00 0x10 0x00
0x00 0x00 0x00 0x04
--- ------------ ---
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.14.0+
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4991888 Bytes = 4.8 MiB
Load Address: 10800000
Entry Point: 10800000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Loading Kernel Image ... OK
Using Device Tree in place at 18000000, end 1800e0eb
1.2G chip, increase VDDARM_IN/VDDSOC_IN
Starting kernel ...
These are the changes to the code:
diff --git a/arch/arm/cpu/armv7/mx6/hab.c b/arch/arm/cpu/armv7/mx6/hab.c
index f58e688b78b8..f7980816e45e 100644
--- a/arch/arm/cpu/armv7/mx6/hab.c
+++ b/arch/arm/cpu/armv7/mx6/hab.c
@@ -136,20 +136,20 @@ uint32_t authenticate_image(uint32_t ddr_start, uint32_t image_size)
hab_rvt_entry = hab_rvt_entry_p;
hab_rvt_exit = hab_rvt_exit_p;
- if (is_hab_enabled()) {
printf("\nAuthenticate image from DDR location 0x%x...\n",
ddr_start);
hab_caam_clock_enable(1);
if (hab_rvt_entry() == HAB_SUCCESS) {
+ printf("hab_rvt_entry success :)\n");
/* If not already aligned, Align to ALIGN_SIZE */
ivt_offset = (image_size + ALIGN_SIZE - 1) &
~(ALIGN_SIZE - 1);
start = ddr_start;
bytes = ivt_offset + IVT_SIZE + CSF_PAD_SIZE;
-#ifdef DEBUG
+
printf("\nivt_offset = 0x%x, ivt addr = 0x%x\n",
ivt_offset, ddr_start + ivt_offset);
puts("Dumping IVT\n");
@@ -162,13 +162,14 @@ uint32_t authenticate_image(uint32_t ddr_start, uint32_t image_size)
(void *)(ddr_start + ivt_offset+IVT_SIZE),
4, 0x10, 0);
+ puts(" --- Status before ---\n");
get_hab_status();
+ puts(" --- ------------- ----\n");
puts("\nCalling authenticate_image in ROM\n");
printf("\tivt_offset = 0x%x\n", ivt_offset);
printf("\tstart = 0x%08lx\n", start);
printf("\tbytes = 0x%x\n", bytes);
-#endif
/*
* If the MMU is enabled, we have to notify the ROM
* code, or it won't flush the caches when needed.
@@ -203,9 +204,12 @@ uint32_t authenticate_image(uint32_t ddr_start, uint32_t image_size)
HAB_CID_UBOOT,
ivt_offset, (void **)&start,
(size_t *)&bytes, NULL);
+ printf("load_addr: %d\n", load_addr);
if (hab_rvt_exit() != HAB_SUCCESS) {
puts("hab exit function fail\n");
load_addr = 0;
+ } else {
+ puts("hab_rvt_exit() success :)\n");
}
} else {
puts("hab entry function fail\n");
@@ -213,15 +217,12 @@ uint32_t authenticate_image(uint32_t ddr_start, uint32_t image_size)
hab_caam_clock_enable(0);
+ puts(" --- status after ---\n");
get_hab_status();
- } else {
- puts("hab fuse not enabled\n");
- }
-
- if ((!is_hab_enabled()) || (load_addr != 0))
- result = 1;
+ puts(" --- ------------ ---\n");
- return result;
+ if (load_addr == 0) return 0;
+ return 1;
}
解決済! 解決策の投稿を見る。
The previous error was generated because I was using different key indexes for validation of the U-Boot image and the uImage. Using the same key index solved the error.
After debugging the problem, I have found that the following code behaves differently:
load_addr = (uint32_t)hab_rvt_authenticate_image(
HAB_CID_UBOOT,
ivt_offset, (void **)&start,
(size_t *)&bytes, NULL);
That returns 0 in closed devices, but != 0 on open devices, using the same U-Boot Image and the same uImage. That is the root cause of the differences.
This is a consistent behaviour, because in open devices allows the device to boot.
I still don't understand the following HAB event, could you help me interpret it?
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0f 0xc0 0x00
0xbe 0x00 0x0c 0x00 0x03 0x17 0x00 0x00
0x00 0x00 0x00 0x50
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_INDEX (0x0F)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)
The previous error was generated because I was using different key indexes for validation of the U-Boot image and the uImage. Using the same key index solved the error.
Hello,
please use Appendix A (Interpreting HAB Event Data from Report_Event() API)
of the “HAB4_API.pdf” in the CST package to get more information about HAB events.
The fact that system boots in any case may mean, that the i.MX6 is not really “closed”.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
thanks for your answer!
Please notice that I am using a properly signed and encrypted U-Boot which does boot a closed device. (The output on the first image shows that the device is in open mode because I tried with both open and closed devices).
The strange behaviour is in the uImage (not the U-Boot image) validation.
I will debug the HAB events to get more information. By the way, I have noticed in posts from other NXP employess a nice formatted HAB interpretation which I think is done by some kind of script. Could you share that script, or any way to automatically interpret HAB events?
Thanks a lot.
Never mind, I just found [U-Boot] [PATCH] iMX: adding parsing to hab_status command !
I will try to debug the HAB events and will update this post, thanks.