VPU support format in i.MX6Dual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VPU support format in i.MX6Dual

1,352 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I have a question about VPU support format in i.MX6Dual.

[Q1]

Please tell me the input data format of H.264 Encoder.

(YUV NV12, YUV XXXX, RGB, etc)

[Q2]

Please tell me the output data format of H.264 Decoder.

(YUV NV12, YUV XXXX, RGB, etc)

Best Regards,

Keita

Labels (6)
0 Kudos
Reply
2 Replies

1,041 Views
Yuri
NXP Employee
NXP Employee

Please refer to section 69.6.3 (Video Codec Processing Buffer Requirement) of the i.MX6 SDL RM.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,041 Views
keitanagashima
Senior Contributor I

Dear Yuri,

Hello.

Thank you for your reply.

I referred to section 69.6.3 (Video Codec Processing Buffer Requirement), but I didn't understand it.

What data format can VPU Encoder(H.264) input internally?

And, what format is it output when decoding H.264 in VPU decoder?

(Ex, YUV NV12, YUV XXXX, RGB, etc)

Best Regards,

Keita

0 Kudos
Reply