VPU issue for Android 5.0 ga using IMX6Q Sabresd board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VPU issue for Android 5.0 ga using IMX6Q Sabresd board

ソリューションへジャンプ
4,368件の閲覧回数
mayqueen
Contributor IV

Hello all:

As title, I don't know why it's very slowly and no smooth when I play the video using  the source code I compiled.

But it looks okay when I use official prebuilt image (only change system.img).

I compare these two system.img, the logcat no different...

How do I fix this issue!? please help me, thanks.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
4,134件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI May

please check that you included freescale codecs in image, refer

to attached document Table 1. Freescale enhanced codecs

This document is included in IMX6_L500_100_ANDROID_DOCS 

i.MX6 Android L5.0.0_1.0.0 BSP Documentation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,135件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI May

please check that you included freescale codecs in image, refer

to attached document Table 1. Freescale enhanced codecs

This document is included in IMX6_L500_100_ANDROID_DOCS 

i.MX6 Android L5.0.0_1.0.0 BSP Documentation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信