VPU Latency on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VPU Latency on i.MX6

Jump to solution
1,574 Views
alexraimondi
Contributor I

I found this Q&A: How is VPU Latency on i.MX6: Q&A: How is VPU Latency on i.MX6


First, I can't access the referenced discussion: VPU Latency i.MX6. Is there a reason it is blocked?

The answer is not clear enough (at least for me ;-) ).

We need to implement an entire encoding/decoding system like this

Camera => encoder => transmission => decoder => display

What end to end (encoder input to decoder output) latency can we achieve?

We need less then 100ms. Is this possible?


Best regards

Alex

Labels (3)
Tags (2)
0 Kudos
1 Solution
833 Views
eaglezhou
NXP Employee
NXP Employee

Hi, Alex

     The 15ms is average value estimated based one noreorder (only I/P frames exist) for 720p,

     In most case, the decoding(or encoding) time for every frame should be less than 15ms.

     Basically, the result is not related with core numbers.

     ixM6DQ/DL/S are all suppose to be ok.

Eagle

View solution in original post

0 Kudos
4 Replies
833 Views
YixingKong
Senior Contributor IV

This discussion has been assgned to an engineer internally.

0 Kudos
833 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Hi, Alex
  
   The latency discussed in #343081 is about the startup latency, is different with your case.
   For your case, I think 100ms is likely possible.
     - camera: assume camera capture one frame at 30ms interval
     - encoder: one frame delay, ~15ms(720p)
     - transmission: ~30 ms ?
     - decoder: one frame delay (suppose no reorder in video syntax), ~15ms(720p)
     - others: ~10ms
 

Eagle

0 Kudos
833 Views
alexraimondi
Contributor I

Hi Eagle

Thank you for your reply

So the encoding/decoding latency of approx. 15ms is a fact? That would be great news ;-)

I guess this is not related to the number of cores in the device, right?

Any suggestion on a hardware platform to use for a proof of concept?

Best regards

Alex

0 Kudos
834 Views
eaglezhou
NXP Employee
NXP Employee

Hi, Alex

     The 15ms is average value estimated based one noreorder (only I/P frames exist) for 720p,

     In most case, the decoding(or encoding) time for every frame should be less than 15ms.

     Basically, the result is not related with core numbers.

     ixM6DQ/DL/S are all suppose to be ok.

Eagle

0 Kudos