General recommendations are as following :
If not using SATA interface and the embedded thermal sensor, the VP and VPH
should be grounded.
Note, the I.MX53 SATA also integrates a temperature sensor. The temperature can
be read by the CPU, and frequency may be scaled-up or scaled-down accordingly.
In case the SATA, including the temperature sensor, is not needed :
- the VP and VPH should be grounded ;
- the rest of the ports both inputs and outputs could be left floating
(SATA_REFCLKM , SATA_REFCLKP , SATA_REXT , SATA_RXM , SATA_RXP , SATA_TXM)
When only temperature sensor is used:
- VP and VPH still need to be connected to 1.2V and 2.5V respectively.
- Reference clock input frequency is not important but needs to be within the
Specified range: 25Mhz to 156.25Mhz