VNC server on Xwayland

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VNC server on Xwayland

1,059件の閲覧回数
JasonFSYang
Contributor II

Dear Sirs,

Is there any recommended vnc server can be run on Xwayland?

I will get error if try to run x11vnc or tigervncserver, 

x11vnc

~$x11vnc :0

x11vnc version: 0.9.16 lastmod: 2019-01-05 pid: 3733
Wayland display server detected.
Wayland sessions are as of now only supported via -rawfb and the bundled deskshot utility. Exiting.

~$vncserver -geometry 1280x1024 -localhost no :0

A X11 server is already running for display :0 on machine localhost.

Any suggestions are welcome

 

0 件の賞賛
返信
1 返信

1,037件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

WayVNC is a VNC server that works with compositors, like Sway, based on the wlroots library. Waypipe works with all Wayland compositors and offers almost-transparent application forwarding, like ssh -X , but currently are not supported in the BSP in this case you will hace to download.

0 件の賞賛
返信