VNC server on Xwayland

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VNC server on Xwayland

1,177 次查看
JasonFSYang
Contributor II

Dear Sirs,

Is there any recommended vnc server can be run on Xwayland?

I will get error if try to run x11vnc or tigervncserver, 

x11vnc

~$x11vnc :0

x11vnc version: 0.9.16 lastmod: 2019-01-05 pid: 3733
Wayland display server detected.
Wayland sessions are as of now only supported via -rawfb and the bundled deskshot utility. Exiting.

~$vncserver -geometry 1280x1024 -localhost no :0

A X11 server is already running for display :0 on machine localhost.

Any suggestions are welcome

 

0 项奖励
回复
1 回复

1,155 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

WayVNC is a VNC server that works with compositors, like Sway, based on the wlroots library. Waypipe works with all Wayland compositors and offers almost-transparent application forwarding, like ssh -X , but currently are not supported in the BSP in this case you will hace to download.

0 项奖励
回复