hello,Community
I would like to connect the LCD module using the J30 connector of the i.MX7Dual evaluation board "iMX7DSABRE".
J30 connector has 2.8V that VLDO4_2V8 of PMIC for LCD module power supply, however VLDO4_2V8 outputs 3.3V.
Is there a way to change this voltage from 3.3V to 2.8V?
Hi Toshiharu
yes one can try to set voltage using pmic regulator APIs described
sect.2.5.2 PMIC PF Regulator attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------