VLC media player for i.MX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VLC media player for i.MX

793 Views
sanjeetkarn
Contributor II

I am trying to cross-compile VLC media player(version-2.1.5) for i.MX based device.

For this there are many dependent libraries required, i built many of them. PulseAudio packages is also among them.

So i downloaded pulseaudio-5.0 and trying to cross-compile it. During cross-compilation of pulseaudio-5.0 i am getting

following error :

/bin/sed: can't read /usr/lib/libXau.la: No such file or directory

libtool: link: `=/usr/lib/libXau.la' is not a valid libtool archive

I found, i have libXau.so library in my rootfs then why libXau.la is required.

On browsing i found that if i will use "lafilefixer --justfixit", it will work and solve my problem.

but how to install  lafilefixer  on my host PC. My host pc is ubuntu-12.04.


Can you help anybody ?

0 Kudos
1 Reply

551 Views
igorpadykov
NXP Employee
NXP Employee

Hi SANJEET

you can look at below links

how to install lafilefixer in ubuntu | Zuppa Answers

http://sources.gentoo.org/cgi-bin/viewvc.cgi/gentoo-x86/dev-util/lafilefixer/files/lafilefixer-0.5

and post on Ubuntu forum

Ubuntu Forums

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos