VGA resolution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VGA resolution

1,186 次查看
DeanHuang
Contributor III

Hi,

I have two question about VGA resolution of iMX53 QSB .

1. According to release_note of iMX53 QSB, VGA device supports 4 resolution:

    1680x1050, 1280x1024, 1024x768, and 800x600

    But, when I set 1680x1050 and 1280x1024 in uboot, they will become 1024x768.

2. Could we change resolution without uboot?

    I means, uboot is not friendly. We should reboot the OS and write command to uboot through UART.

    Have any other ways to set resolution?

    ps: xrandr is not worked...

标签 (1)
0 项奖励
回复
1 回复

924 次查看
KrishnaPavan
Contributor II

Hi,

What file have you changed to set the resolution?

Can you please specify?

0 项奖励
回复