VFS: Mounted root (yaffs2 filesystem) on device 31:1. Freeing init memory:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VFS: Mounted root (yaffs2 filesystem) on device 31:1. Freeing init memory:

978 Views
1518177561
Contributor I

I  want to use yaffs2  for  root filesystem,kernel configure for yaffs2 (Miscellaneous filesystems.png,Boot options.png) ,ltib -m config for yaffs2 (ltib config option.png).

I run  nandwrite -p  /dev/mtd1 /mnt/sdcard/rootfs.yaffs2 command down the yaffs2 filesystem to the nandflash, when start the freescale  imx287 board .  I eagerly  look forward to help.   the follow error appear:

VFS: Mounted root (yaffs2 filesystem) on device 31:1.
Freeing init memory: 160K
------------/sbin/init------------
Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
Backtrace:
[<c00344c8>] (dump_backtrace+0x0/0x114) from [<c04126e0>] (dump_stack+0x18/0x1c)
r7:00000013 r6:c0056014 r5:c002a228 r4:c0577ad8
[<c04126c8>] (dump_stack+0x0/0x1c) from [<c041275c>] (panic+0x78/0xf4)
[<c04126e4>] (panic+0x0/0xf4) from [<c0030604>] (init_post+0xbc/0xe8)
r3:00000000 r2:c7656d00 r1:c7656e00 r0:c04c1cf7
[<c0030548>] (init_post+0x0/0xe8) from [<c00084fc>] (kernel_init+0x12c/0x174)
r5:c002a228 r4:c0576c20
[<c00083d0>] (kernel_init+0x0/0x174) from [<c0056014>] (do_exit+0x0/0x6dc)
r5:c00083d0 r4:00000000

Labels (1)
0 Kudos
Reply
0 Replies