VESA display timing on i.MX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VESA display timing on i.MX6UL

1,163件の閲覧回数
paulschoenke
Contributor III

I have a design with the i.MX6UL and am trying to and change the display timings to a standard VESA aspect such as the following, but I'm not getting the proper timing output that I would expect:

 

                                                timing0 {

                                                clock-frequency = <40000000>;

                                                hactive = <800>;

                                                hfront-porch = <40>;

                                                hsync-len = <128>;                                          

                                                hback-porch = <88>;

                                                vactive = <600>;                                               

                                                vfront-porch = <1>;

                                                vsync-len = <4>;

                                                vback-porch = <23>;                                       

                                                hsync-active = <0>;

                                                vsync-active = <0>;

                                                de-active = <1>;

                                                pixelclk-active = <0>;

                                                };

 

With the above settings, when we measure the pixel clock, we get 36 MHz instead of 40 MHz, similar ~10% errors at 640x480 and 1024x768).

The numbers above were produced correctly except for the clock frequency and the slower clock frequency also generated lower display refresh which it was at 54Hz instead of 60Hz due to slower pixel clock.  It has to do something with PLL setting in order to generate proper PLL clock.

Any feedback or input is welcomed and appreciated!

Thanks!

Paul

ラベル(1)
0 件の賞賛
返信
1 返信

1,054件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Please let me know what files and BSP are used in the case ?

Regards,

Yuri.

0 件の賞賛
返信