VDIC combine in i.MX6 solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VDIC combine in i.MX6 solo

1,527 Views
suryag
Contributor II

I would like to combine two graphical planes(RGB format) using VDIC combiner feature in i.MX6 solo.

As per data sheet, VDI_plane1 (IDMAC CH 26) and VDI_plane 3 (IDMAC CH 25) input data can be combine and output (Combined data) can be obtained from IDMAC CH 5, when VDI_CMB_EN bit is set IPU_VDI_C register in VDIC module, But it is not working.


Is anybody worked on VDIC combiner feature? Could you help me to solve the VDIC combiner issue.



Thanks & Regards

Surya


Labels (3)
Tags (2)
1 Reply

1,174 Views
chuanyanyin
Contributor III

I have encounter the same issue, could nxp give a example of VDI conbining? We don't know how vdi works if we don't have a example. BTW,I use linux to do the program.

0 Kudos
Reply